Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Unable to Connect to PSoC 64 MCU after "Erase Chip" Operation in J-Flash Tool - KBA232539

Unable to Connect to PSoC 64 MCU after "Erase Chip" Operation in J-Flash Tool - KBA232539

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: VitaS_81           Version: **

Background: This issue occurs because during the “Erase Chip" operation, the whole flash of device is erased including the Cypress Secure Bootloader allocated in the main flash area, which is not protected from erasing.

Solution: Use the "Erase Sectors" operation in J-Flash tool instead of “Erase Chip".

If you have already performed an Erase Chip operation, reprogram the Cypress Secure Bootloader into PSoC 64 MCU by using the re-provisioning instructions from PSoC® 64 Secure MCU Secure Boot SDK User Guide.

 

0 Likes
522 Views