Employee
Jul 02, 2020
11:40 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jul 02, 2020
11:40 PM
USB-Serial: UART Flow Control under CDC - KBA230578
Version: **
Translation - Japanese: USC-シリアル:CDC下でのUARTフロー制御 – KBA230578 - Community Translated (JA)
Question:
Why does UART Flow Control not work for USB-Serial Devices configured as Communication Device Class (CDC)?
Answer:
Native Windows/Linux/Mac CDC driver does not support UART Flow Control for the USB-Serial devices.
The Hardware Flow Control feature for UART is a custom implementation present in the Cypress CDC driver (CypressUsbConsoleWindowsDriver64). To use the feature, the USB-Serial device must be bound to the Cypress driver.
You can install Cypress CDC and Vendor driver for USB-Serial devices from the SDK installation available at USB-Serial Software Development Kit Page.
Rate this article: