Community Manager

Community Manager
Jun 29, 2022
02:20 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
Type of Xtal used for ECO in TRAVEO™ II Family (KA-03403)
Crystal Unit and Ceramic Resonator can be used for ECO. TRAVEO™ II has a built-in ECO gain control amplifier and can support various Xtals by setting the amplifier parameters.
Amplifier parameters are calculated using the specifications of Xtal. For more details, see the “Clocking System” section of the Architecture Technical Reference Manual and the ECO User Guide. If the calculation result of an Xtal is out of the specified range, the corresponding Xtal cannot be used.
Note: This applies to the following series of TRAVEO™ II MCUs:
- CYT2 Series
- CYT3 Series
- CYT4 Series
Labels
Rate this article: