Traveo™ S6J3110/3120/3400 MCUs: Partial Wakeup Trigger Signal Not Generated - KBA223671
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Author: kotaroh_86 Version: **
Question:
In Traveo™ S6J3110/3120/3400 MCUs, why is the Partial Wakeup Trigger (PWUTRG) signal not generated in partial wakeup mode?
Answer:
This may happen if the PWU_PWUC register, which is set after power on, is cleared by events such as software reset or hard reset except for a power-on reset. Check the register setting and ensure that the register is set correctly even when a reset other than the power domain reset (*1) is applied. For details of the related register, see the registers of the RESET chapter in the Technical Reference Manual from the following link.
S6J3110: http://www.cypress.com/documentation/technical-reference-manuals/s6j3110-series-32-bit-microcontroll...
S6J3120: http://www.cypress.com/documentation/technical-reference-manuals/s6j3120-series-32-bit-microcontroll...
S6J3400: http://www.cypress.com/documentation/technical-reference-manuals/32-bit-microcontroller-traveotm-fam...
*1: Power domain reset factor from Partial Wakeup mode is different for different products.
S6J3110/3120: Power Domain 2 / 3 / 6_0 reset
S6J3400: Power Domain 2 reset