TRAVEO™ T2G Automotive Body Controller - FAQ – CLOCKING - KBA232509
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Home Page: TRAVEO™ T2G Automotive Body Controller - FAQ – CDC
13. Clocking
13.1. How do I configure ECO?
- Set the ECO pins in the default High-Z state. No additional port/pin configurations are required.
- Other configurations involve registers CLK_ECO_PRESCALE, CLK_ECO_CONFIG, and CLK_ECO_CONFIG2 as mentioned in Section 18.2.2, “External Crystal Oscillator (ECO)” in the Traveo™ II Automotive Body Controller Entry Family Architecture Technical Reference Manual (TRM) (002-19314 Rev. *E).
13.2. As the peripherals in TRAVEO™ T2G are organized as group and slaves, how would I know the clock tree mapping for these peripheral with respect to group and slave?
For the mapping of the group and slave for the peripheral, see the ‘Peripheral I/O Map’ section in the device datasheet.
Example: In CYT2B7 devices, the SCB belongs to group 6 with seven slaves, so PERI_GR6_CLOCK_CTL will be used to set the divider and PERI_GR6_SL_CTL will be used to enable/disable the slave clock gate.
13.3. Are there any precautions to be taken while switching the clock source?
It takes four cycles of the originally selected clock to switch away from it and the original clock should not be disabled during this time.
13.4. What happens if ECO is short circuited or not populated?
On start up or boot the default clock is the IMO. ECO can be configured as the clock source later in the application code. Regardless of whether ECO is set as the clock source later, cm0+ applies the ECO trims during the boot up process along with other regulator trim values.
Under ideal conditions when the ECO is configured as the clock source in the application code, it would be set as the clock source after its amplitude has stabilized. If ECO is not populated, the amplitude stabilization timeout occurs, the ECO_OK and ECO_READY would fail and the application code would be stuck in a while loop.
while(SRSS->unCLK_ECO_STATUS.stcField.u1ECO_OK == 0ul);
while(SRSS->unCLK_ECO_STATUS.stcField.u1ECO_READY == 0ul);
If the above fields fail, there is no ‘fall back’ mechanism that would allow the MCU to continue operation using IMO.
13.5. How many HF paths are allowed to connect to one PLL?
Ideally, all HF paths (CLK_HFx) can be configured to derive their source from any PLL clock path (CLK_PATHx). There are no limitations. However, multiple clock paths enable you to scale the frequency required for the operation of specific IPs shown in Table 46 (clock specifications) of the datasheet. With all CLK_HFx deriving clock from a single clock path, the Pre-dividers of each HF path would be able to provide certain limited frequencies and lose out on scalability.