Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Transition Time from PSS STOP Mode to RUN Operation in Traveo S6J3200 Series MCUs – KBA227496

Transition Time from PSS STOP Mode to RUN Operation in Traveo S6J3200 Series MCUs – KBA227496

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: ShusakuS_56       Version: **

Translation - Japanese: Traveo S6J3200シリーズMCUのPSS STOPモードからRUN操作への移行時間 – KBA227496 - Community Translated (JA)

Question:

How long is the recovery time from STOP mode (Shutdown mode)?

Answer:

It takes at 22 ms (maximum) + the power-up time of external 1.2 V regulator that is automatically controlled by the PSC_1 pin.

For more details on this sequence, see "3.4. Operations after Reset Release" in the 32-Bit Microcontroller Traveo™ Family S6J32XX Series Hardware Manual Platform Part.

For more details on the PSC_1 pin, see “CHAPTER 3: Product Description” in the 32-bit Microcontroller Traveo™ Family S6J3200 Series Hardware Manual.

SHUS

0 Likes
255 Views
Contributors