Thermal Information for Cypress Flash370i CPLDs
Anonymous
Not applicable
Jan 01, 2012
04:47 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jan 01, 2012
04:47 PM
Question: 1. What is the Theta JA value for the 37xi? 2. What is the Theta JC value for the 37xi?
Answer:
The Thermal information is located in the table that follows:
Device | Package Type | Theta JA (C/W) | Theta JC (C/W) |
CY7C371i | 44-Lead Thin Plastic Quad Flatpack | 62 | 17 |
CY7C371i | 44-Lead Plastic Leaded Chip Carrier | 54 | 18 |
CY7C372i | 44-Lead Plastic Leaded Chip Carrier | 38 | 16 |
CY7C372i | 44-Pin Thin Quad Flatpack | 56 | 6 |
CY7C373i | 84-Lead Plastic Leaded Chip Carrier | 35 | 16 |
CY7C373i | 100-Pin Thin Quad Flatpack | 50 | 7 |
CY7C374i | 84-Lead Plastic Leaded Chip Carrier | 35 | 16 |
CY7C374i | 100-Pin Thin Quad Flat Pack | 29 | 5 |
CY7C374i | 84-Pin Ceramic Leaded Chip Carrier | 50 | 7 |
CY7C375i | 160-Lead Thin Quad Flatpack | 34 | 7 |
CY7C375i | 160-Pin Grid Array | 24 | 3 |
CY7C375i | 160-Pin Ceramic Quad Flatpack | 30 | 5 |
Please be noted our entire Cypress CPLD product are Obsolete and not recommended for new design and development. For more information on CPLD product, please visit our webpage: http://www.cypress.com/go/cpld
Labels
- Tags:
- phys
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous