Community Manager

Community Manager
Jun 29, 2022
03:04 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
Thermal Data in TRAVEO™ II Family (KA-03407)
The thermal parameters (ƟJa, ƟJB, ƟJc) used to characterize the packages for CYT2B series are shown below.
For example: TVII-B-E-2MB device.
TQFP-64: ƟJa = 36.5 °C/W, ƟJb = 31.5 °C/W, ƟJc = 7.4 °C/W
TQFP-80: ƟJa = 31.7 °C/W, ƟJB = 26.0 °C/W, ƟJc = 6.2 °C/W
TQFP-100: ƟJa = 28.6 °C/W, ƟJB = 20.9 °C/W, ƟJc = 5.3 °C/W
The above thermal resistance values are also described in the Packaging section of the Datasheet. See the Packaging section for the thermal resistance of other series as well.
Note: This applies to the following series of TRAVEO™ II MCUs:
- CYT2 Series
- CYT3 Series
- CYT4 Series
Labels
Rate this article: