Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Test firmware for PSoC™ 6 Bluetooth® LE RF Certification – KBA235365

lock attach
Attachments are accessible only for community members.

Test firmware for PSoC™ 6 Bluetooth® LE RF Certification – KBA235365

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: PSoC™ 6 Bluetooth® LE RF認証用テストファームウェア - KBA235365 
Version: **


You can use the test firmware attached with this article for all regulatory testing and Bluetooth® qualification testing of PSoC™ 6 Bluetooth® LE devices and modules.

It provides the features needed to support the Receiver Blocking test of EN 300 328 v2.1.1 and Python scripts with unified APIs for Bluetooth® LE 2-wire and MTK interfaces.

The integrated test code is a single firmware image that supports the following features:

  • Regulatory test support with a single-button interface
  • Bluetooth® LE 2-wire command support
  • MTK commands through the UART port

For further details, see the documentation in the folder.

Note :

For using the ‘RXC’ MTK command for ETSI tests, change the high-frequency clock source to ECO or ExtClk or AltHF. In the project workspace explorer of PSoC Creator, go to .cydwr > clocks tab > click ‘Edit clock’ > Source clocks tab > Disable IMO and set ECO or ExtClk or AltHF as source (Figure 1). This is done to accurately time the receiver window.

BinduPriya_G_0-1655202819359.png

 
Figure 1      Clock settings

Attachments
0 Likes
1145 Views