Employee
ArunKumarChoul
Employee
Oct 21, 2021
09:37 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
Termination of unused pins for CY27410/CY27430 – KBA233899
Version: **
Note:
For spec numbers 001-00001 to 001-99999, the KBA number is five digits; for spec numbers 002-xxxxx, add '2' to make it a 6-digit number. For example, for spec 002-12345, the KBA number is 002-212345 to distinguish it from KBA12345 for spec 001-12345.
Question:
How to terminate the unused power pins for CY27410 or CY27430 ?
Answer:
We will use the pin out for CY27410 to understand better.
Power supply pins like VDDIO-D2 or VDDIO-S2 can be left open/floating, if they are unused in the application.
Rate this article: