Termination Resistors for Type-C to Legacy Ports
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
What are the termination resistors required on the configuration channel (CC) line for Type-C to legacy cable and Type-C to legacy adapter assemblies?
The following Table 1 provides details of the termination resistors required on the CC line for various Type-C to legacy cable/adapter designs.
Table 1: Termination resistors for Type-C to Legacy cable/adapter assemblies
Design |
Termination on CC Line |
USB Type-C to USB3.1 Standard Standard-A Cable Assembly |
Rp1 |
USB Type-C to USB2.0 Standard Standard-A Cable Assembly |
Rp1 |
USB Type-C to USB3.1 Standard Standard-B Cable Assembly |
Rd2 |
USB Type-C to USB2.0 Standard-B Cable Assembly |
Rd2 |
USB Type-C to USB2.0 Mini-B Cable Assembly |
Rd2 |
USB Type-C to USB3.1 Micro-B Cable Assembly |
Rd2 |
USB Type-C to USB2.0 Micro-B Cable Assembly |
Rd2 |
USB Type-C to USB 3.1 Standard-A Receptacle Adapter Assembly |
Rd2 |
USB Type-C to USB 2.0 Micro-B Receptacle Adapter Assembly |
Rp1 |
Notes:
1. The A5 pin (CC) of the USB Type-C plug should be connected to VBUS through a resistor, Rp. The following figure illustrates the functional model for a legacy host port connected to a UFP. This model has an adapter that presents itself as a host to the UFP. The adapter is either a USB Standard-A legacy plug or a USB Micro-B legacy receptacle on one end and the USB Type-C plug on the other end connected to a UFP. For more information about the functional description and value of Rp, refer to section 4.5.3.2.2 and Table 4-10 of the USB Type-C Specification Revision 1.1.
Figure 1: The functional model for a legacy host port connected to a UFP.
2. The A5 pin (CC) of the USB Type-C plug should be connected to GND through a resistor, Rd. The following figure illustrates the functional model for a DFP connected to a legacy device port. This model has an adapter present as a UFP to the DFP. The adapter has a USB Type-C plug on one end connected to the DFP, and either a USB Standard-B plug, USB Micro-B plug, USB Mini-B plug, or a USB Standard-A receptacle on the other end. For more information about the functional description and value of Rd, refer to section 4.5.3.2.1 and Table 4-14 of the USB Type-C Specification Revision 1.1.
Figure 2: The functional model for a DFP connected to a legacy device port.
- Tags:
- ccg1
- ccg2
- cmg1
- cypd1xxx
- cypd2xxx
- ez-pda ccg1 type-c port controller
- ez-pda ccg2 type-c cable controller
- high speed
- Legacy Ports
- termination resistors
- type-c
- type-c to legacy adapter
- type-c to legacy cable
- usb 3.0
- usb-c and power delivery