Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TRAVEO™ T2G MCU: Using interrupt in CM0+ causes HardFault – KBA236874

TRAVEO™ T2G MCU: Using interrupt in CM0+ causes HardFault – KBA236874

Infineon_Team
Employee
Employee
50 replies posted 25 likes received 25 replies posted

Community Translation: TRAVEO™ T2G MCU: CM0+ で割り込みを使用すると HardFault が発生する – KBA236874

Version: **

While running the code in CM0+ core, note that IRQ0 and IRQ1 interrupts are reserved only for internal system calls; if interrupts are to be used in the code, use IRQ2 or IRQ3.

Refer to the “Nonvolatile memory programming” section of the TRAVEO™ T2G architecture TRM for more information.

Note:  This KBA applies to the following series of TRAVEO™ T2G MCUs:

  • CYT2 Series
  • CYT3 Series
  • CYT4 Series
0 Likes
236 Views