Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TRAVEO™ T2G Automotive Body Controller - FAQ – RTC - KBA232509

TRAVEO™ T2G Automotive Body Controller - FAQ – RTC - KBA232509

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Home Page: TRAVEO™ T2G Automotive Body Controller - FAQ – CDC

19. RTC

 

19.1. What is the tolerance of RTC in TRAVEO™ T2G device?

The tolerance of RTC depends on the tolerance of RTC Input Clock basically. The Watch Crystal Oscillator (WCO), LPECO, or ILO can be used for RTC Input Clock.

If the external oscillator is used for the RTC Input Clock, the accuracy of external oscillator is RTC tolerance. If ILO is used for RTC Input Clock, the accuracy of ILO is the tolerance of RTC.

See the device datasheet for ILO AC Specifications.

19.2. Does RTC in TRAVEO™ T2G device support temperature calibration?

RTC in TRAVEO™ T2G device supports 512 Hz, 1 Hz, and 2 Hz of calibration waveform output. The accuracy of the RTC is improved by calibrating the WCO or LPECO. The CLK_LF can also be calibrated. See Section 21.7 WCO/LPECO Calibration of the TRAVEO™ T2G Automotive Body Controller Entry Family Architecture Technical Reference Manual (002-19314 Rev. *F).

If the temperature calibration has to be considered, it is necessary to monitor Calibration waveform at RTC_CALL output pin for each experimental temperature (for example, -40℃, 25℃, 105℃) condition and compare it with an ideal reference waveform for each temperature condition.

0 Likes
571 Views