Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TLE9210x, TLE9563/4: What is the meaning of the gain drift?

TLE9210x, TLE9563/4: What is the meaning of the gain drift?

IFX_Publisher2
Community Manager
Community Manager
Community Manager
25 likes received 1000 replies posted First like given

Community Translation: TLE9210x, TLE9563/4: ゲインドリフトの意味はなんですか?

The gain drift is the drift of the gain after calibration.
For example, the gain of the current sense amplifier is calibrated at 25 °C with a two-point calibration (i.e. using two load currents).
The gain drift is the drift resulting from the device ageing and from the temperature drift (from Tj = -40°C to 150°C).

0 Likes
192 Views