Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TLE5009: Angle error deviation for errors above 5 degrees.

TLE5009: Angle error deviation for errors above 5 degrees.

Infineon_Team
Employee
Employee
50 replies posted 25 likes received 25 replies posted

In the application note equation 11 and 12 are only suitable, if parameter measurement deviations of less than 5° are expected.
For the Min/Max method, investigations showed that measured angle errors above 5° have a higher angle error than calculated.
To cover all possible boundary conditions, an empirical method is described in the enhanced orthogonality calculation.

0 Likes
50 Views