Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TLE4922 Magnetic Speed Sensor: What is the minimum air gap?

TLE4922 Magnetic Speed Sensor: What is the minimum air gap?

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: TLE4922磁気速度センサー: 最小エアギャップはどのくらいですか?(KA-01300)

In the https://www.infineon.com/dgdl/Infineon-TLE4922-XIN-F-DS-v01_00-EN.pdf?fileId=5546d46258fc0bc1015988a... datasheet the parameter “minimum air gap” is specified and verified at a certain wheel. The reference wheel is mentioned in the datasheet. Due to restrictions of the measurement setup the minimum air gap verified is 0.5mm.
In case of no run out of the target wheel and accurate positioning, a minimum air gap of 0.0mm can work. In the application a minimum air gap of 0.0mm is possible as long as BLR (parameter “Linear Region”) is not exceeded.
Be aware the tooth of the toothed wheel increases flux density and in combination with a strong back bias magnet the minimum air gap might be 0.5mm or even 1.0mm. Typically this should not be an issue since TLE4922 is overmolded by customer mold-compound.

0 Likes
273 Views