Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TLE 4205G XUMA1: Observing oscillating output

TLE 4205G XUMA1: Observing oscillating output

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: TLE 4205G XUMA1: 発振出力を観察する(KA-01012)

If the voltage at all inputs is approx.1.5V or VS-5V, the output oscillates. This is because the inputs do not have built-in hysteresis, only an offset. The device is not optimized for such an application. Therefore, if the difference between the inputs is greater than the offset, the outputs will oscillate. Why this is happening exactly at 1.5V and Vs-5V cannot be explained on device level. This may depend on the application.

0 Likes
145 Views