Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TCRAM Contents in PSS Mode in Traveo S6J3XXX Series MCUs – KBA228169

TCRAM Contents in PSS Mode in Traveo S6J3XXX Series MCUs – KBA228169

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: ShusakuS_56           Version: **

Translation - Japanese: Traveo™ S6J3XXX シリーズ MCU の PSS モードでの TCRAM の内容について - KBA228169 - Community Translated (JA)

Question:

If the MCU wakes up from PSS (Power Saving State), the RAM value is undefined. Why?

Answer:

In PSS, TCRAM power is not supplied. Therefore, the TCRAM value is undefined.

If you have data that you want to keep in PSS, save it in BackupRAM. BackupRAM has an area where power is supplied even in PSS.

For details, see the “Low Power Consumption” section in the following documents.

- S6J3110: S6J3110 Series 32-bit Microcontroller Traveo™ Family Hardware Manual
- S6J3120: S6J3120 Series 32-bit Microcontroller Traveo™ Family Hardware Manual
- S6J3200: 32-Bit Microcontroller Traveo™ Family S6J32XX Series Hardware Manual Platform Part
- S6J3300/3350/3360/3370/3400/3510: 32-Bit Microcontroller Traveo Family S6J33xx, S6J34xx, S6J35xx Series Hardware Manual Platform Part

Notes: This KBA applies to the following series of Traveo MCUs:

S6J3110

S6J3120

S6J3200

S6J3300

S6J3350

S6J3360

S6J3370

S6J3400

S6J3510

0 Likes
475 Views
Contributors