- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
TCPWM Block of CY8C62x4 Devices - KBA231254
Community Translation: CY8C62x4デバイスのTCPWMブロック - KBA231254
Version: **
Question:
What are the differences in the TCPWM block of the CY8C62x4 devices compared to other PSoC 6 MCU devices?
Answer:
Note: This article presumes the reader has an in-depth knowledge of the TCPWM block in PSoC 6 MCU devices and its various operational modes.
CY8C62x4 (PSoC 6 MCU with 256K flash) devices have a new version of the TCPWM block that is targeted mainly for motor control applications, and Field-Oriented Control (FOC) in particular.
The following is a list of major changes that support this application and their intended example usage:
- Second Capture / Compare function
The CY8C62x4 TCPWM block has two compare/capture registers (CC0 and CC1), while the block in other PSoC 6 MCU devices have only one. The functionalities of both CC0 and CC1 are the same. A typical application is the generation of asymmetric PWM signals with a lower CPU load (compared to generation using a single CC function). These signals are widely used in motor control applications for enabling single-shunt current measurement.
- Immediate PWM kill
The kill input is synchronized with a faster peripheral clock, while in other PSoC 6 MCU devices, it is a slow counter clock. This gives a better response time in emergency situations to kill the PWM signal, such as a short circuit in the motor control application.
- Second kill input trigger
The TCPWM block in CY8C62x4 has two kill input triggers, while the block in other PSoC 6 MCU devices have only one. A common kill input can be selected from the trigger multiplexer block, for allowing synchronous stop/kill operation of multiple PWMs. The dedicated ADC out-of-range trigger can be selected as the additional kill input for allowing real-time hardware stop of a PWM signal.
- Independent dead times for line and complementary line output signals
In CY8C62x4, the PWM line and complementary line output signals can be configured to have different dead times, while in other PSoC 6 MCUs, both outputs have a common dead time. Dead time is used to prevent short circuits in motor control applications. This feature gives more control over the gap between outputs.
- Compare match events can be enabled/disabled independently while counter is up or down counting
The CY8C62x4 TCPWM block has two compare/capture registers (CC0 and CC1) as explained previously. When the counter is configured to work in up/down mode (counts up until period and then counts back down to zero), the compare match event for CC0 and CC1 can be independently enabled or disabled for either up counting or down counting. This feature is used for asymmetric PWM signal generation.
Resources: Device Datasheets, Technical Reference Manuals
- Subscribe to RSS Feed
- Mark Article as New
- Mark Article as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Hi I have some questions regarding TCPWM blocks of CY8C62x4 devices.
As you mentioned in this thread, this device family could use CC1 as a second compare for PWM output line.
but in this reference manual for CY8C6xx4, it should be set [7:6] bitfield of the TCPWM0_GRP0_CNT0_TR_PWM_CTRL register.
But in the register reference manual of the cy8c6xx4 device, these bitfields are marked as NONE.
Which one is correct information ?
and also I would like to know that CY8C6144 devices also could use this special features that you described? or only for the CY8C6244 devices?
thanks,
Oliver
- Subscribe to RSS Feed
- Mark Article as New
- Mark Article as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Hi I found an answer about my question above myself.
In CY8C6xx4 devices, there are 32bit TCPWM and 16bit TCPWM.
second compare value is not available on 32bit TCPWM but it is available in 16bit TCPWM.
please refer to the below picture.