Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Switching to External Clock (EXTCLK) in PSoC 4100S Plus Device in PSoC Creator 4.2 – KBA229081

Switching to External Clock (EXTCLK) in PSoC 4100S Plus Device in PSoC Creator 4.2 – KBA229081

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: EktaN_26           Version: **

Translation - Japanese: PSoC Creator 4.2 で PSoC 4100S Plus デバイスのクロックを外部クロック (EXTCLK) に切り替える - KBA229081- Community Translate...

PSoC 4100S Plus devices always start up using the IMO; the ExtClk can only be enabled in the user application during runtime. Also, the device cannot be started from reset which is clocked by EXTCLK.

Do the following to switch to EXTCLK:

  1. Open the project In PSoC Creator.
  2. In the project, click the Clocks tab under Design Wide Resources and click Edit Clock.
  3. Under High Frequency Clocks tab, enable both ExtClk and IMO.
  4. Set the frequency for both IMO and ExtClk.
  5. Set the source of the HFClk to IMO as shown in  Figure 1 below. P0[6] is the default pin used for providing input to the external clock.

pastedImage_1.png

Figure 1: Clock Configuration

You can switch to the external clock during run time with the CySysClkWriteHfclkDirect(CY_SYS_CLK_HFCLK_EXTCLK) API function. This will switch the input of the HFClk from IMO to ExtClk.

For PSoC 4100S Plus devices, you must manually enable the srss.ext_clk HSIOM connection for P0[6] pin using the following code in main.c:

#include "project.h"

int main(void)

{

CY_SET_REG32((void *)(CYREG_HSIOM_PORT_SEL0), (CYVAL_HSIOM_IO0_SEL_ACT_0 << (6 * 4))); /* HSIOM_IO0_SEL_ACT_0 */

CY_SET_REG32((void *)(CYREG_GPIO_PRT0_PC), (CY_SYS_PINS_DM_DIG_HIZ  << (6 * 3))); /* High Impedance Digital */

/* 6 is a pin number, 3 and 4 are bitfield widths */

    CySysClkWriteHfclkDirect(CY_SYS_CLK_HFCLK_EXTCLK);

     for(;;)

{

    /* Perform the desired function */

}

}

Note: The new clock source must be running and stable before calling this function. If the SysClk frequency increases during device operation, call CySysFlashSetWaitCycles() with the appropriate parameter to adjust the number of clock cycles the cache will wait before sampling data comes back from the flash. If the SysClk frequency decreases, call CySysFlashSetWaitCycles() to improve the CPU performance. See CySysFlashSetWaitCycles() description in PSoC 4 System Reference Guide for more information.

0 Likes
547 Views
Contributors