Version: *A
Translation - Japanese: ImageCraft™コンパイラとHi-TechC®コンパイラの切り替え– KBA83349 - Community Translated (JA)
Question: How do you switch between the ImageCraft™ and Hi-Tech C® compilers?
Answer:
To switch between the two compilers, modify the compiler options and review the migration document.
Modify the compiler options in PSoC® Designer™:
Tools > Options > Build > Compiler
or
Project > Settings > Build > Compiler
Refer to the “HiTech_to_ImageCraft_Migration” guide, which is included with PSoC Designer (Help > Documentation > Compiler and Programming Documents).
You can also refer to the ImageCraft “C Language Compiler User Guide” (in the same location) for more detail on features that affect project migration.
Note: Cypress no longer provides the HI-TECH Lite compiler for PSoC in PSoC Designer. Instead, a free C compiler from ImageCraft is provided.