Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Streaming Data through Isochronous or Bulk Endpoints on EZ-USB® SX2™ - KBA211686

Streaming Data through Isochronous or Bulk Endpoints on EZ-USB® SX2™ - KBA211686

Anonymous
Not applicable

Version: **

Translation - Japanese: EZ-USB® SX2™上のアイソクロノスまたはバルクエンドポイントを介したデータのストリーミング - KBA211686 - Community Translated (JA)

Question:

How do I configure SX2 for streaming data through bulk or isochronous endpoints?

Answer:

EZ-USB SX2 is a serial interface engine (SIE)–only device without any RAM for code download. It needs an external master to initialize its registers and enable the device to enumerate. SX2 only buffers the data from the peripheral and sends it to the host over USB and vice versa. SX2 cannot modify the data received from either the peripheral or the host before committing it to the destination. By configuring the endpoints appropriately in SX2, it can be enabled to stream data to/from the external master from/to the USB Host. Streaming data through SX2 is equivalent to streaming data through EZ-USB FX2LP configured for Slave AUTO mode operation.

Endpoints in SX2

SX2 supports one control endpoint (EP0) and four configurable data endpoints (EP2, EP4, EP6, and EP8), like EZ-USB FX2LP, and occupies the dedicated endpoint RAM. Data endpoints are configurable as bulk, interrupt, or isochronous; double, triple, or quad buffered endpoints sharing the 4-KB FIFO buffer space (Figure 1).

Figure 1. High-Speed Endpoint Configurations

1.png

The default endpoint memory configuration at power-on reset is as follows:

  • EP2: Bulk OUT, 512 bytes, 2x buffered
  • EP4: Bulk OUT, 512 bytes, 2x buffered
  • EP6: Bulk IN, 512 bytes, 2x buffered
  • EP8: Bulk IN, 512 bytes, 2x buffered

Endpoint register configuration

SX2 contains configuration registers that control the size, length, and direction of its endpoint buffers. The external master has to write the appropriate values into these registers for the endpoints to function according to the descriptors. For example, to configure Endpoint 2 as an IN endpoint, in addition to writing the descriptors for Endpoint 2 appropriately, the SX2 command register EP2CFG has to be written with a corresponding value to configure the direction of the SX2 Endpoint 2 buffer as IN. For a list of the SX2 registers, refer to the SX2 datasheet.

Consider one example endpoint configuration as follows:

  • Endpoint 2: Bulk OUT, 512 bytes, 2x buffered in high-speed mode
  • Endpoint 4: Bulk IN, 512 bytes, 2x buffered in high-speed mode
  • Endpoint 6: Interrupt IN, 1024 bytes, 2x buffered in high-speed mode

The values to be written into the registers to achieve this configuration follow (note that the register names as given in the SX2 datasheet are listed as comments alongside the values):

0xAA,     //IFCONFIG // MHz=1=48 ASYNC=1 FLAGD=1
0xA8,     //FLAGA - fixed EP2EF, FLAGB - fixed EP6EF
0xFD,     //FLAGC - fixed EP4FF, FLAGD - fixed EP8FF
0x00,     //POLAR // all signals active low
0xA2,     //EP2CFG // Set Dir OUT
0xE0,     //EP4CFG // Set Dir IN
0xFA,     //EP6CFG // Set Dir IN
0x00,     //EP8CFG // Invalid Endpoint
0x02,     //EP2PKTLENH // Zerolen=0 Wordwide=0
0x00,     //EP2PKTLENL
0x02,     //EP4PKTLENH // Zerolen=0 Wordwide=0
0x00,     //EP4PKTLENL
0x22,     //EP6PKTLENH // Zerolen=1 Wordwide=0
0x00,     //EP6PKTLENL
0x22,     //EP8PKTLENH // Zerolen=1 Wordwide=0
0x00,     //EP8PKTLENL
0x82,     //EP2PFH
0x00,     //EP2PFL
0x82,     //EP4PFH
0x00,     //EP4PFL
0x82,     //EP6PFH
0x00,     //EP6PFL
0x82,     //EP8PFH
0x00,     //EP8PFL
0x01,     //EP2ISOINPKTS
0x01,     //EP4ISOINPKTS
0x01,     //EP6ISOINPKTS
0x01,     //EP8ISOINPKTS
0xFF     //INTENABLE

Similarly for isochronous endpoint configuration, the appropriate values must be set for the corresponding EPxCFG register. Refer to the SX2 datasheet for the EPxCFG register field definitions.

Note: SX2 was not designed to support dynamic modification of these endpoint configuration registers. If the application needs the ability to change endpoint configurations after the device has already enumerated with a specific configuration, expect some delay in accessing the FIFOs after changing the configuration. For example, after writing to EP2PKTLENH, you must wait for at least 35 µs, measured from the time the READY signal is asserted, before writing to the FIFO. This delay varies for different registers and is not specified.

SX2 can successfully enumerate with the required endpoint configuration after the appropriate values are written to the SX2 configuration registers and the descriptors are loaded into SX2.

External interface

The payload data to the external master is automatically transferred from the USB domain to the peripheral or interface domain and transferred over the Slave FIFO interface under the control of the external master. Similarly, the payload data sent by the external master to SX2 over the Slave FIFO interface is automatically transferred to the USB domain from the peripheral or interface domain. The slave FIFO architecture uses the endpoints (in the endpoint RAM) as FIFO memories that are controlled by FIFO control signals (IFCLK, CS#, SLRD, SLWR, SLOE, PKTEND, and FIFOADR[2:0]). SX2 has three address pins (FIFOADR[2:0]) that are used to select either the FIFOs or the command interface (Table 1). Refer to the SX2 datasheet for further details on how to access the Slave FIFO interface (synchronously or asynchronously) from the external master.

Table 1. FIFO Address Line Settings

                                                                                                                                                                                                                                              

Address/
    Selection
EndpointFIFOADR2FIFOADR1FIFOADR0
FIFO2EP2000
FIFO4EP4001
FIFO6EP6010
FIFO8EP8011
COMMANDEP0/SX2
    registers
100
RESERVED-101
RESERVED-110
RESERVED-111

Thus, correct endpoint configuration and correct addressing from the external master to select the appropriate endpoint will enable seamless data streaming through that endpoint.
Refer to other Knowledge Base Articles on SX2 here.

0 Likes
707 Views
Contributors