Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

State of the RXSC/D* signal while VLTN is asserted for the CY7C9689A

lock attach
Attachments are accessible only for community members.

State of the RXSC/D* signal while VLTN is asserted for the CY7C9689A

Anonymous
Not applicable
Question: What is the state of the RXSC/D* signal while VLTN is asserted for the CY7C9689A?

 

Answer:

RXSC/D* will remain unchanged when VLTN is asserted.
In the pin description of VLTN on page 7 of the datasheet, it states that "When VLTN is asserted the values on the output DATA and COMMAND buses remain unchanged" and as RXSC/D* comes from the same output buffer as the DATA and COMMAND buses it behaves the same.

Useful Link:
TAXI-compatible HOTLink Transceiver (Attached Below 38-02020_0C_V)

Attachments
0 Likes
395 Views
Contributors