Community Manager
Jun 24, 2021
05:25 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jun 24, 2021
05:25 AM
Set infinite retry for VBUS OCP fault - KBA233337
Community Translation: VBUS OCPフォルトに対する無限リトライ設定 - KBA233337
Version: **
The CCGx Power SDK 3.5 example firmware provides two ways:
1. Change the Retry count from 2 (default value) to 255 by using the EZ-PD™ configuration utility, and then save the configuration into firmware .hex/.cyacd file directly. You can also replace the config.c file in the firmware project and rebuild it.
2. Change the config.h file in firmware project directly without configuration table changes on Over Current Protection and rebuild the firmware project.
- Locate the config.h file (under the solution folder of Header Files group):
- Enable delayed infinite fault recovery.
Labels
Rate this article: