SRAM tape and reel requirement
Anonymous
Not applicable
Mar 05, 2011
02:37 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Mar 05, 2011
02:37 AM
Question:
What is the tape and reel requirement for Cypress SRAM's?
Answer:
First, the part are sealed on the reel by tape and, although not hermetically sealed, it will offer additional shelf exposure time. However, this time is neither measured nor guaranteed. Second, the tape and reel materials can not withstand the standard bake temperature of 125C. However, if the parts do need to be baked then a lower temperature, but longer time, may be acceptable to reach level moisture content specification. The tape and reel bake requirement is temperature of less than 60C and a time limit of 24hrs.
Labels
- Tags:
- 1 mb quad spi nvsram
- 16mb nvsram- replacement for battery-backed sram and mram
- 4 mb f-ram
- async fast srams
- async micropower (mobla) srams
- dual-port srams
- f-ram parallel
- f-ram processor companion
- f-ram serial
- fifos
- mobl dual-ports
- nonvolatile ram
- nvsram parallel
- nvsram serial
- quadporta dse srams
- synchronous srams
- wafer & die
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous