Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

SPI clock frequency for Cypress SPI NOR flash device – KBA226830

SPI clock frequency for Cypress SPI NOR flash device – KBA226830

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Author: SudheeshK_26           Version: **

Question:

Is it necessary to keep the SPI clock frequency for Cypress SPI NOR flash devices always constant? Is it possible to change clock frequency within an SPI operation (CS# cycle)?

Answer:

It is not necessary to keep the SPI clock frequency constant always for Cypress SPI NOR flash devices. User can perform different SPI operations at different frequencies, if they are within the operating frequency range. But, it is not recommended to change SPI clock frequency within an SPI operation (CS# cycle).Changing SPI clock frequency within an SPI operation will violate the below datasheet specs (from S25FL512S datasheet).

tWH, tCH

Clock High Time 

45% PSCK

ns

tWL, tCL

Clock Low Time 

45% PSCK

ns

However, it is possible to have breaks in SCK signal between sending each byte.

For example:

  1. It is possible to make SCK signal LOW for a longer duration in between sending command and address during a program operation.
  2. It is possible to make SCK signal LOW for a longer time after sending RDSR command and before reading the SR value back.

Below waveform diagrams illustrate these two scenarios.

Figure1: Single byte program operation (Includes WREN command at the first CS# cycle in below diagram)

pastedImage_1.png

Figure 2: Single byte read operation

pastedImage_18.png

SPI clock frequency should be constant for each byte transaction (command or address or data) during a SPI operation (8 clock cycles).

0 Likes
789 Views
Contributors