cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

SMPTE standards supported by HOTLink family

Anonymous
Not applicable

SMPTE standards supported by HOTLink family

Question: 1)How can I use the HOTLink1 parts in a SMPTE-259M application?2)Does Cypress have a part that supports the SMPTE 310M video standard?

 

Answer:

Within the HOTLink1 family of parts there was a SMPTE 259M video chipset. The CY7B9234/9334 (Transmitter/Receiver) and the CY7C9235/9335 (Srambler/Descrambler) was a SMPTE 259M solution, currently they are Obsolete. These parts supported the following Levels:
1. SMPTE 259M Level C (270 Mbps, 525/625component)
2. SMPTE 259M Level D (360 Mbps, 525/625component)

In addition, a cable driver and equalizer will need to be used. Information on how to use the HOTLink 1 parts in a SMPTE-259M application can be found in two application notes (links are attached below). Adaptive Equalizers and Cable Drivers can be purchased from National Semiconductor. The parts we recommend are:
CLC006 Serial Digital Cable Driver with Adjustable Outputs
CLC007 Serial Digital Cable Driver with Dual Complementary Outputs
CLC014 Adaptive Cable Equalizer for High-Speed Data Recovery


Neither the HOTLink product family nor any other Cypress products support the SMPTE 310M standard for the following reasons:

- SMPTE-310M uses bi-phase mark encoding, HOTLink uses the 8B/10B encoding scheme,
- SMPTE-310M requires a synchronous serial interface to carry MPEG-2 transport bit streams at rates of up to 40Mb/s, HOTLinks lowest serial rate is 50Mb/s therefore is not compliant.

For more detailed information please see the SMPTE-310M spec and compare it to HOTLink specifications.


0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Jul 01, 2011 08:07 AM
Updated by:
Anonymous
 
Contributors