Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

S6BT112A Behavior when Power Supply Voltage Is Between 4.7 V and 5.3 V – KBA228013

S6BT112A Behavior when Power Supply Voltage Is Between 4.7 V and 5.3 V – KBA228013

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: SadaharuK_26          Version: **

The minimum value of recommended operating power supply voltage of S6BT112A is 5.3 V.

The maximum value of the low-level power-on reset threshold voltage is 4.7 V.

The chip is designed to work normally when the power supply voltage is between 4.7 V and 5.3 V.

Note that the electrical characteristics under 4.7 V ~ 5.3 V power supply voltage is not guaranteed by shipment test.

0 Likes
229 Views
Contributors