Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Reset Factor of PSC_1 Pin in Traveo™ S6J3200 MCU - KBA225721

Reset Factor of PSC_1 Pin in Traveo™ S6J3200 MCU - KBA225721

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Author: kotaroh_86           Version: **

Translation - Japanese: Traveo™S6J3200 MCUのPSC_1ピンのリセット要因 - KBA225721 - Community Translated (JA)

Question:

What are the factors that cause low level voltage in PSC_1 pin?

Answer:

The following factors cause a low level voltage in PSC_1 pin:

  • Power-on reset
  • RAM retention low-voltage detection reset
  • Internal power supply low-voltage detection reset
  • External power supply low-voltage detection reset1
  • Extended internal power supply low-voltage detection reset
  • INITX
  • Illegal mode detection reset
  • Hardware watchdog reset
  • Power Domain reset 2

1 This reset is activated by EXVRSTCNT=0 in the system special setting register (SYSC0_SPECFGR).

For more details, see Chapter 4: Reset 3.2.3. Reset of External Power Supply Control for the signal EX12VRST in 32-Bit Microcontroller Traveo™ Family S6J32XX Series Hardware Manual Platform Part.

0 Likes
244 Views
Contributors