Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Reload Value of 32-bit Reload Timer after Reload Timer Stopped in Traveo S6J3XXX Series MCUs – KBA227520

Reload Value of 32-bit Reload Timer after Reload Timer Stopped in Traveo S6J3XXX Series MCUs – KBA227520

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: shusakus_56           Version: **

Translation - Japanese: Traveo S6J3XXXシリーズMCUでリロードタイマが停止した後の32ビットリロードタイマのリロード値 – KBA227520 - Community Translated (JA)

Question:

Is the reload value (RLTn_TMRLR register) held after reload timer stopped in the S6J3XXX series?

Answer:

Yes. The reload value is held after the reload timer stops. You don’t need to set it again when the reload counter restarts. For more details, refer to 32-bit Reload Timer section in the TRM from the following link:

S6J3120: S6J3120 Series 32-bit Microcontroller Traveo™ Family Hardware Manual

S6J3200: 32-Bit Microcontroller Traveo™ Family S6J32XX Series Hardware Manual Platform Part

S6J3300/3350/3360/3370/3400/3510: 32-Bit Microcontroller Traveo Family S6J33xx, S6J34xx, S6J35xx Series Hardware Manual Platform Part

This setting applies to the following series of Traveo MCUs:

  • S6J3120
  • S6J3200
  • S6J3300
  • S6J3350
  • S6J3360
  • S6J3370
  • S6J3400
0 Likes
285 Views
Contributors