Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Recommended frequency for enCoRe III CY7C64215 to run the CPU at 3.3V

Recommended frequency for enCoRe III CY7C64215 to run the CPU at 3.3V

Anonymous
Not applicable

Recommended frequency for enCoRe III CY7C64215 to run the CPU at 3.3V

Question: What is the recommended frequency for enCoRe III CY7C64215 to run the CPU at 3.3V ?

 

Answer:

At 3.3V, the recommended frequency maximum is 12MHz.

CPU needs a minimum of 4.75V Vdd in order to work properly at 24Mhz.

0 Likes
Contributors