cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

R/B pins for the CY7C68023

Anonymous
Not applicable

R/B pins for the CY7C68023

Question: What is the functionality of multiple R/B pins in CY7C68023?

 

Answer:

The NX2LP has two R/B pins to support a protocol known as "interleave". This allows the NX2LP to work with a different NAND flash chip (or die in a chip) while another is busy. When interleave is not used (almost all cases), both of the R/B signals on the NX2LP need to be tied together so that proper ready/busy operation is detected.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Mar 28, 2011 02:30 AM
Updated by:
Anonymous
 
Contributors