Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Programming Multiple PSoC® 1 Devices in Parallel and Timing Details - KBA85717

Programming Multiple PSoC® 1 Devices in Parallel and Timing Details - KBA85717

Anonymous
Not applicable

Version: *A

Translation - Japanese:  複数のPSoC®1デバイスの並列プログラミングおよびタイミングの詳細 - KBA85717 - Community Translated (JA)

Question:
Can I program multiple PSoC® 1 devices at the same time, and how much time does it take to program a single device?

Answer:
For high-volume production it is necessary that multiple devices be programmed at the same time. It is possible to program multiple PSoC 1 devices in parallel. A range of third-party programmers is available to program multiple PSoC 1 devices simultaneously. The following table lists the programmers available from Cypress-qualified third-party vendors.

                                                                                                                                    

Vendor Product Software version Web Link
Hi-Lo Systems ALL-200 v1.44 http://www.hilosystems.com.tw/
    en/programmers/all-200
ALL-200G v1.44 http://www.hilosystems.com.tw/
    en/programmers/all-200g
RPM Systems MPQ 4 Port
    Programmer
Rev 1.11.1
    (Firmware 2.14)
http://www.rpmsys.com/psoc_programmer.htm
Elnec BeeProg2 PG4UW 2.77 http://www.elnec.com/products/universal-
    programmers/beeprog2/#multiprogramming
System General T9600 v1.38r http://www.sg.com.tw/instruGP/t9600_C.asp

 

PSoC 1 is programmed using the ISSP protocol. For general information on programming a PSoC 1 device refer to the following webpage: http://www.cypress.com/node/92446. The time required to program different PSoC 1 devices depends upon the host programmer as well as the target PSoC 1 device. The following table gives the timing details of various PSoC 1 families programmed with different programmers.

                                                                                                                                                                                                                                        

PSoC 1 Family Flash
    Memory
MiniProg 1 MiniProg 3

Touch Tuning
Bridge

Elnec System
    General
Hi Lo
29x66 32k 33.5 27.7 27.7 30.2 27.7 34
27x43 16k 9.5 6.9 6.9 7.6 6.9 13.4
21x34 8k 10.1 10.1 9.1 8.5 8.1 11.4
20xx6/A 32k 17.2 13.4 10.8 17.3 17.2 14.3
TM(A/G)300 32k 15.5 8.8 8.8 Not Supported 11.2 11.7
0 Likes
505 Views