Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Problem Registering Keil License: Error Code 9939 - KBA225736

Problem Registering Keil License: Error Code 9939 - KBA225736

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Author: DheerajK_81          Version: **

Community Translation: Community Translation - Problem Registering Keil License: Error Code 9939 - KBA225736

Question:
The new Cypress PK51 license registration on PSoC Creator™ failed. How can I resolve this and get my project to compile?

Answer:
As of November 2018, the Cypress 4K version of the Keil C51 compiler (PK51) has expired. New registrations for this license displays the error “code 9939” as shown in Figure 1.

 

Figure 1: Error Code 9939

  pastedImage_0.png

Cypress is working towards addressing this issue as soon as possible and getting the licenses renewed. Once the license is renewed, it will be notified on this page. Alternately, you can use the workarounds suggested below.

 

Suggested Workarounds

  1. Users who have installed PSoC Creator recently can continue to compile the projects for a trial period of 30 days with the standard Keil 2K evaluation version which comes by default, but it will not be able to compile applications with code size > 2 KB. If the trial period has expired, the compiler generates the error “INCORRECT LICENSE ID CODE (LIC) IN 'TOOLS.INI’”.
  2. Users who are reinstalling PSoC Tools on the same machine can reuse the unexpired license by modifying the tools.ini file as specified in step 2 of the Registration of Keil Compiler in PSoC Creator.
  3. Users who do not fall in the above two categories must wait until end of December 2018 tentatively for the renewed license.
  4. Users can also opt to purchase a full version of the Keil tools. Click here to purchase the license.
0 Likes
717 Views
Comments
DheerajK_81
Moderator
Moderator
Moderator
First comment on KBA First comment on blog 5 questions asked

The licenses have been made available for a week, deadline being December 22nd to help everyone resume work if they have been stalled because of this. Please make use of this opportunity to get the license as soon as possible.

What happens after December 22nd?

We are in pursuit of renewing the license and it will be available soon like it was before, but since we do not want your work to be affected until that, the licenses are being made available for a week as a temporary solution.

Please refer the following link for registration:

PSoC Creator™ - Keil Compiler Registration - KBA83314

Regards,

Dheeraj