cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Power supply decoupling required for HOTLink products

Anonymous
Not applicable

Power supply decoupling required for HOTLink products

Question: What special power supply decoupling is required for HOTLink products?

 

Answer:

HOTLink requires no special considerations for power-supply bypassing beyond that normally associated with high-speed logic. This typically includes the use of a ground plane, a Vcc plane, and bypassing using multiple RF quality chip capacitors. Each of the ground pins of a HOTLink IC should connect directly to the ground plane using short (<6 mm) traces and vias. All of the Vcc pins should connect to a Vcc area under the HOTLink, which is then connect to the board Vcc through a single via. Connect one 10- to 22-nF capacitor (based on operating character clock rate) for each Vcc pin directly from the pin to GND. For more information see the "Using Decoupling Capacitors" application note.

Useful Link:
Using  Decoupling Capacitors

 

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Dec 19, 2008 12:00 AM
Updated by:
Anonymous
 
Contributors