Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Power Supply Terminal and Reference Voltage Terminal of A/D Converter in Traveo™ S6J3110/3120/3400 Series MCUs - KBA218103

Power Supply Terminal and Reference Voltage Terminal of A/D Converter in Traveo™ S6J3110/3120/3400 Series MCUs - KBA218103

Anonymous
Not applicable

Version: **

Translation - Japanese: Traveo™ S6J3110/3120/3400シリーズMCUのA/D変換の電源供給端子およびリファレンス電圧端子 - KBA218103 - Community Translated (JA)

Question:

Are AVCC0 and AVCC1 connected to each other internally?

Are AVRH0 and AVRH1 connected to each other internally?

What happens if one of those pins is open?

Answer:

AVCC0 and AVCC1 are not connected internally.

AVRH0 and AVRH1 are not connected internally.

If the AVCC pin open, the ADC result is undefined. This may lead to damage to the MCU because of latch up.

If the AVRH pin open, the ADC result is undefined.

312 Views
Contributors