Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Power Sequence for PSoC 6 – KBA227565

Power Sequence for PSoC 6 – KBA227565

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: LinglingG_46           Version: **

Translation - Japanese: PSoC 6 の電源投入シーケンス - KBA227565 - Community Translated (JA)

Question:
Is there a power sequence required for different supplies such as VDDD, VBACKUP, VDDIO, and VDDA in PSoC® 6?

Answer:
No, power sequence is not required.

VDDD, VBACKUP, VDDIO, and VDDA do not have any sequencing limitation and can establish in any order. The presence of VDDA without VDD or VDDD can cause some leakage from VDDA. However, VDDA will not drive any analog or digital output.  All VDDA pins in packages that offer multiple VDDA supply pins must be shorted externally (on the PCB). Note that the system will not exit reset until both VDDD and VDDA are established. However, the system will not wait for other supplies to establish.

0 Likes
279 Views
Contributors