Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Port Configuration for PSS Mode in Traveo S6J3XXX Series MCUs - KBA222863

Port Configuration for PSS Mode in Traveo S6J3XXX Series MCUs - KBA222863

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Version: *A

Translation - Japanese: Traveo™ S6J3XXX シリーズ MCU の PSS モードのポート構成について - KBA222863 - Community Translated (JA)

Question:

Do S6J3110/3120/3200/3300/3350/3360/3370/3400/3510 Traveo™ series MCUs have any recommended port settings for the lowest power consumption in PSS mode?

Answer:

These Traveo series MCUs have no special recommendation for the port setting in PSS mode. However, the input port is usually set to HI-Z with the PIE bit of the PPC_PCFGRiij register. When that bit is set to `0`, the input port becomes HI-Z internally. For the output port, the output level is set to LOW normally. It is recommended to keep the same level requested by the interfacing device in PSS mode, if the facing device needs to input HIGH or LOW in PSS mode. To set an output port as HI-Z, change the direction of the ports to "Input".

Note: This KBA applies to the following series of Traveo MCUs:

  • S6J3110
  • S6J3120
  • S6J3200
  • S6J3300
  • S6J3350
  • S6J3360
  • S6J3370
  • S6J3400
  • S6J3510
360 Views