Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Platform Files for CYBLE-013025-EVAL

lock attach
Attachments are accessible only for community members.

Platform Files for CYBLE-013025-EVAL

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Which platform files should be used for CYBLE-013025-EVAL kit in the WICED™ Smart IDE?

 

CYBLE-013025-EVAL kit includes a fully integrated and certified Bluetooth Low Energy (BLE) wireless module solution (CYBLE-013025-00). Details of the platform files used for this kit in WICED Smart SDK are presented below.

Make the following changes to the WICED Smart SDK to start using the CYBLE-013025-EVAL kit platform:

  1. Download CYBLE_013025_EVAL Platform files.zip attached to this KBA.
  2. Save and extract the downloaded file in your computer.
  3. Navigate to CYBLE_013025_EVAL Platform files > CYBLE_013025_EVAL and copy this folder.
  4. Paste this folder in WICED Smart SDK folder path …\WICED-Smart-SDK\Platforms\. Figure 1 shows the location of folder in the WICED Smart SDK.

    Figure 1
    KBA220379-1.JPG

  5. Navigate to CYBLE_013025_EVAL Platform files > include _ platforms > CYBLE_013025_EVAL and copy this folder
  6. Paste this folder in WICED Smart SDK folder path … \WICED-Smart-SDK\include\Platforms\. Figure 2 shows the location of folder in the WICED Smart SDK installation.

    Figure 2
    KBA220379-2.JPG

A sample make target to build a project in WICED Smart IDE for this evaluation kit is shown below: 

hello_sensor-CYBLE_013025_EVAL download

Attachments
3887 Views