Placing Code at Absolute Location in Flash
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Question: How do I place code at an absolute location in PSoC flash?
Response:
1. Using C:
We can do this using the ‘#pragma’ directive in PSoC Designer. Suppose we need to define a relocatable code area called ‘my_code_area’ in the memory locations 0x3800 to 0x3FFF. The following steps are to be followed to do this:
1. Declare a custom area in the PSoC flash memory which will contain the user-written code using the ‘#pragma’ directive in the main.c file of your PSoC Designer project. You can insert the code you wish in this area as follows:
#pragma text:my_code_area // Place following code in custom area in flash
// add your code here
#pragma text:text // Place following code in default area
‘my_code_area’ can be any user-defined name.
2. A file called custom.lkp can be created in the root folder of the project, which can contain Linker commands. A typical use for employing the custom.lkp capability would be to define a custom relocatable code area. The code was placed in the custom area in the previous step. Now, add the following line to the custom.lkp file which will place the custom area in the address range 0x3800 to 0x3FFF.
-bmy_code_area:0x3800.0x3FFF
2.Using assembly language:
This can also be done using the ‘AREA’ assembler directive. ‘AREA’ defines where code or data is placed in RAM or flash by the Linker. You have to follow the steps given below:
1. Declare a custom area in PSoC flash memory which will contain the user-written code using the ‘AREA’ assembler directive in the main.asm file of you PSoC Designer project. You can insert your code in this area as follows:
AREA my_code_area(ROM,ABS,CON)
ORG 2000h
_my_code_area_start: */insert your code here
(Please refer to the Assembly Language Compiler Guide for more details)
Note:
The PSoC flash contains the following seven areas:
lit
func_lit
· psoc_config
· UserModules
· idata
· text
· top
(Please refer C Language Compiler User Guide for more details about these sections of flash)
These are not absolute areas, i.e., the space they occupy differ from project to project. For instance, if you add a user module to your project in PSoC Designer, the space occupied by the UserModules will increase and this will be compensated for by other sections of flash. If we define these areas rigidly, we lose this flexibility which is undesirable. So in the custom.lkp file, we only have to define the custom area we want to use to insert the code as shown above with ‘my_code_area’.
-
This widget could not be displayed.Anonymous