Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Pin Mapping Differences Between the EZ-BLE™ PSoC® Evaluation Board (CYBLE-224116- EVAL) and the BLE Pioneer Kit (CY8CKIT-042-BLE) - KBA216235

Pin Mapping Differences Between the EZ-BLE™ PSoC® Evaluation Board (CYBLE-224116- EVAL) and the BLE Pioneer Kit (CY8CKIT-042-BLE) - KBA216235

Anonymous
Not applicable

Version: **

Translation - Japanese: EZ-BLE™ PSoC®評価ボード(CYBLE-224116- EVAL) と BLEパイオニアキット(CY8CKIT-042-BLE) とのピンマッピングの違い - KBA216235 - Com...

Question:

Are there differences between the pins exposed on J1 and J2 headers of the EZ-BLE PSoC Evaluation Board (CYBLE- 224116-EVAL) and the pins expected by the J10 and J11 headers on the BLE Pioneer Kit (CY8CKIT-042-BLE)?

Answer:

Yes, there are differences in pin mapping between exposed pins of EZ-BLE PSoC Evaluation Board and BLE Pioneer Kit. The EZ-BLE PSoC Evaluation Board quick start guide explains how to use the board with the BLE Pioneer Kit and the differences in pin mapping. This is also explained below.

Figure 1: J10 and J11 Headers on BLE Pioneer Kit

1.png

Figure 1: J10 and J11 Headers on BLE Pioneer Kit

Figure 2 shows EZ-BLE PSoC Evaluation Board (CYBLE-224116-EVAL), which is a fan-out board for the EZ-BLE PSoC Module (CYBLE-224116-01).

2.png

Figure 2: EZ-BLE PSoC Evaluation Board (CYBLE-224116-EVAL) Pinout

The EZ-BLE PSoC Evaluation Board’s J2 and J1 are plugged in to J11 and J10 headers of BLE Pioneer Kit respectively.

The EZ-BLE PSoC Module exposes a subset of the GPIOs that are expected on the BLE Pioneer Kit. Therefore, the evaluation board for the module has several pins that do not map to any port of the module. In addition, some pins exposed on the J1 and J2 headers of the evaluation board differ from the pins expected on the J10 and J11 headers of the BLE Pioneer Kit. A table showing the complete pin mapping and highlighting differences is shown below. The table specifies NC (No Connect) for the pins that are not available on the evaluation board.

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                              

CY8CKIT-042-BLE J11 HeaderCYBLE-224116-EVAL J2 HeaderCY8CKIT-042-BLE J10 HeaderCYBLE-224116-EVAL J1 Header
VDDDVDD*VDDAVDD*
VREFVREFVDDRVDDR
XRESXRESGNDGND
GNDGNDGNDGND
P0_0NCP2_0P0_1**
P0_1NC**P2_1P2_1
P0_2NCP2_2P2_2
P0_3NCP2_3P2_3
P0_4P0_4P2_4P2_4
P0_5P0_5P2_5P2_5
P0_6P0_6P2_6P2_6
P0_7P0_7P2_7P1_0**
P1_0NC**P3_0P3_0
P1_1P1_1P3_1P3_1
P1_2P1_2P3_2NC**
P1_3P1_3P3_3NC**
P1_4P1_4P3_4P3_4
P1_5P1_5P3_5P3_5
P1_6NCP3_6P3_6
P1_7NCP3_7P3_7
P4_0NC***
P4_1NC***
P5_0P5_0
P5_1P5_1

*EZ-BLE PSoC Module shorts the digital and analog power rails of PSoC 4 BLE (highlighted rows in blue)
**Pins differ from the pins expected on the BLE (highlighted rows in yellow)
***The EZ-BLE PSoC Module has the P4_0 pin however this is connected to the Cmod capacitor on the EZ-BLE PSoC Evaluation Board (and similarly P4_1 pin is connected to Ctank capacitor) and is not exposed on the J1 header.

Note: The EZ-BLE PSoC Module is supported on PSoC® CreatorTM 4.0 and later versions. While the GPIOs available on the EZ-BLE PSoC Module and consequently on the EZ-BLE PSoC Evaluation Board are limited, every functionality available on a PSoC 4 BLE silicon is available on the EZ-BLE PSoC Module. The only exception is the CapSense® Gestures Component that handles one- and two-finger gestures. This Component is not available on the EZ-BLE PSoC Module.

Headers (on CYBLE-224116-EVAL): Usage description

                                              

HeadersUsage description
J3 

It is used to short VDDD and VDDR.

  

Note: J3 can be ignored for usage if customers insert CYBLE-224116-EVAL into CY8CKIT-042-BLE since VDDD and VDDR are shorted in CY8CKIT-042-BLE. However, if customers use the CYBLE-224116-EVAL separately, customer need to short J3 based on application requirement.

J4 

MiniProg3 10-pin Programming Header

Applicable Kits:

                                                                          

EZ-BLE PSoC Evaluation BoardPRoC BLE ModulesPSoC 4 BLE Modules
CYBLE-224116-EVALCY5671CY5674CY8CKIT-142CY8CKIT-141
YESNONONONO
0 Likes
628 Views
Contributors