Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Pin Mapping Differences Between the EZ-BLE™ PRoC™ Evaluation Board (CYBLE-212020-EVAL) and the BLE Pioneer Kit (CY8CKIT-042-BLE) - KBA212838

Pin Mapping Differences Between the EZ-BLE™ PRoC™ Evaluation Board (CYBLE-212020-EVAL) and the BLE Pioneer Kit (CY8CKIT-042-BLE) - KBA212838

Anonymous
Not applicable

Version: *A

Translation - Japanese: EZ-BLE™ PRoC™評価ボード(CYBLE-212020-EVAL) と BLEパイオニアキット(CY8CKIT-042-BLE) とのピンマッピングの違い - KBA212838 - Comm...

Question:

What are the differences between the pins exposed on J1 and J2 headers of the EZ-BLE PRoC Evaluation Board (CYBLE-212020-EVAL) and the pins expected by the J10 and J11 headers on the BLE Pioneer Kit (CY8CKIT-042-BLE)?

Answer:

Yes, there are differences between the pins exposed. The EZ-BLE PRoC Evaluation Board quick start guide explains how to use the board with the BLE Pioneer Kit and the differences in pin mapping. This is also explained below.

Figure 1 shows the J10 and J11 headers on the BLE Pioneer Kit.

pastedImage_4.png

Figure 1: J10 and J11 headers on BLE Pioneer Kit

The EZ-BLE PRoC Evaluation Board can be plugged on to these headers as shown in Figure 2.

pastedImage_14.png

Figure 2: EZ-BLE PRoC Evaluation Board plugged on BLE Pioneer Kit

Figure 3 shows the pinout and details of the EZ-BLE PRoC Evaluation Board (CYBLE-212020-EVAL), which is a fan-out board for EZ-BLE PRoC Modules (CYBLE-212020-01).

pastedImage_26.png

Figure 3: EZ-BLE PRoC Evaluation Board (CYBLE-212020-EVAL) Pinout

The EZ-BLE PRoC Module exposes a subset of the GPIOs that are expected on the BLE Pioneer Kit. Therefore, the evaluation board for the module has several pins that do not map to any port of the module. In addition, some pins exposed on the J1 and J2 headers of the evaluation board differ from the pins expected on the J10 and J11 headers of the BLE Pioneer Kit. A table showing the complete pin mapping and highlighting differences is shown below. The table specifies NC (No Connect) for the pins that are not available on the evaluation board.

CY8CKIT-042-BLE

J11 Header

CYBLE-212020-EVAL

J2 Header

CY8CKIT-042-BLE

J10 Header

CYBLE-212020-EVAL

J1 Header

VDDD

VDD*

VDDA

VDD*

VREF

VREF

VDDR

VDDR

XRES

XRES

GND

GND

GND

GND

GND

GND

P0_0

NC

P2_0

P2_0

P0_1

NC

P2_1

P0_5**

P0_2

NC

P2_2

P2_2

P0_3

NC

P2_3

P2_3

P0_4

NC

P2_4

P2_4

P0_5

NC

P2_5

P0_4**

P0_6

P0_6

P2_6

P2_6

P0_7

P0_7

P2_7

P3_5**

P1_0

P1_0

P3_0

NC

P1_1

NC

P3_1

NC

P1_2

NC

P3_2

P3_2

P1_3

NC

P3_3

P3_3

P1_4

P1_4

P3_4

P3_4

P1_5

P1_5

P3_5

P3_5

P1_6

P1_6

P3_6

P3_6

P1_7

P1_7

P3_7

P3_7

P4_0

NC***

P4_1

NC

P5_0

P5_0

P5_1

P5_1

*EZ-BLE PRoC Module shorts the digital and analog power rails of PRoC BLE (highlighted rows in blue)

**Pins differ from the pins expected on the BLE (highlighted rows in yellow)

***The EZ-BLE PRoC Module has the P4_0 pin however this is connected to the Cmod capacitor on the EZ-BLE PRoC Evaluation Board and is not exposed on the J1 header.

Note: The EZ-BLE PRoC Module is supported on PSoC® CreatorTM 3.3 SP2 and later versions. While the GPIOs available on the EZ-BLE PRoC Module and consequently on the EZ-BLE PRoC Evaluation Board are limited, every functionality available on a PRoC BLE silicon is available on the EZ-BLE PRoC Module. The only exception is the CapSense® Gestures Component that handles one- and two-finger gestures. This Component is not available on the EZ-BLE PRoC Module.

Applicable Kits:

EZ-BLE PRoC Evaluation Board

PRoC BLE Modules

PSoC 4 BLE Modules

CYBLE-212020-EVAL

CY5671

CY5674

CY8CKIT-142

CY8CKIT-141

YES

NO

NO

NO

NO

Headers (on CYBLE-212020-EVAL): Usage description

Headers

Usage description

J3

It is used to short VDDD and VDDR.

Note: J3 can be ignored for usage if customers insert CYBLE-212020-EVAL into CY8CKIT-042-BLE since VDDD and VDDR are short in CY8CKIT-042-BLE. However, if customers use the CYBLE-212020-EVAL separately, customer need to short J3 based on application requirement.

J5

P5.0 and P5.1 are available for debug purposes (no jumper usage intended here).

J6

It is used to short P3.5 of CYBLE-212020-01 module to either/both of P3.5 and P2.7 of CY8CKIT-042-BLE.

0 Likes
688 Views
Contributors