Employee
Jun 09, 2020
05:17 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jun 09, 2020
05:17 AM
PSoC 6シリーズのSIMOにおけるスイッチングノード - KBA229738 - Community Translated (JA)
Community Translated by YoTa_1693656 Version: **
質問:
PSoC® 6シリーズのSinge Input Multiple Output(SIMO)のスイッチングノードは、VIND1とVINDのうち、どちらでしょうか?
回答:
PSoC 6シリーズは、スイッチング(降圧)コアレギュレータを搭載しています。
そのデバイスに搭載されているスイッチングコアレギュレータは1系統の入力から2系統の出力を生成するSIMOレギュレータです。
SIMOを使用ためには、図1に示す通りVID1端子とVID2端子の間に外部インダクタの接続が必要です。また、スイッチングノードもVIND1でなければなりません。
図1. PSoC 63デバイスのVID1とVID接続
Rate this article: