Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC® 5 Support in PSoC Creator™ 3.0 and Later – KBA92931

PSoC® 5 Support in PSoC Creator™ 3.0 and Later – KBA92931

Anonymous
Not applicable
Version: **

 

Question: Why is PSoC® 5 not listed in PSoC Creator™ 3.0 and later?

 

Answer:

PSoC Creator no longer supports the PSoC 5 silicon starting from PSoC Creator 3.0. The PSoC 5 devices have been functionally replaced by equivalent PSoC 5LP devices.

If you open a project that targets an obsolete part, the dialog shown in Figure 1 will appear.

Figure 1. Obsolete Device Dialog

The dialog suggests the appropriate new part number, and clicking OK will update the project to the functionally-equivalent device. This will automatically create a backup of the original design. Clicking Cancel will abort the opening of the project.

Note that if you wish to migrate PSoC 5 designs on Cypress® development kits to the new kits (with PSoC 5LP devices) the new target part number should be CY8C5868AXI-LP035. This is different from the part listed below (CY8C58568AXI-LP032) because the 035 part also supports the CAN interface, which was needed in the development kit. In this situation, click (choose another replacement) to launch the Device Selector dialog and switch to the LP035 part.

Table 1 lists all the obsolete parts and their functional equivalents.

Table 1. Obsolete Parts and Their Functional Equivalents

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                         
    Device Family    PSoC 5    PSoC 5LP
    CY8C52 = CY8C52LP    CY8C5246AXI-054    CY8C5266AXI-LP033
         CY8C5246LTI-029    CY8C5266LTI-LP029
         CY8C5247AXI-051    CY8C5267AXI-LP051
         CY8C5247LTI-089    CY8C5267LTI-LP089
         CY8C5248AXI-047    CY8C5268AXI-LP047
         CY8C5248LTI-030    CY8C5268LTI-LP030
    CY8C53 = CY8C54LP    CY8C5365AXI-043    CY8C5465AXI-LP043
         CY8C5365LTI-104    CY8C5465LTI-LP104
         CY8C5366AXI-001    CY8C5466AXI-LP002
         CY8C5366LTI-053    CY8C5466LTI-LP085
         CY8C5367AXI-108    CY8C5467AXI-LP108
         CY8C5367LTI-003    CY8C5467LTI-LP003
         CY8C5368AXI-106    CY8C5468AXI-LP106
         CY8C5368LTI-026    CY8C5468LTI-LP026
    CY8C54 = CY8C56LP    CY8C5466AXI-064    CY8C5666AXI-LP004
         CY8C5466LTI-063    CY8C5666LTI-LP005
         CY8C5467AXI-011    CY8C5667AXI-LP006
         CY8C5467LTI-007    CY8C5667LTI-LP008
         CY8C5468AXI-018    CY8C5668AXI-LP010
         CY8C5468LTI-037    CY8C5668LTI-LP014
    CY8C55 = CY8C58LP    CY8C5566AXI-061    CY8C5866AXI-LP021
         CY8C5566LTI-017    CY8C5866LTI-LP022
         CY8C5567AXI-019    CY8C5867AXI-LP024
         CY8C5567LTI-079    CY8C5867LTI-LP028
         CY8C5568AXI-060    CY8C5868AXI-LP032
         CY8C5568LTI-114    CY8C5868LTI-LP038
479 Views
Contributors