- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
PSoC 4 Flash Emulate EEPROM with Non-blocking Feature – KBA233049
Community Translation: ノンブロッキング機能を備えたPSoC 4フラッシュ エミュレーション EEPROM – KBA233049
Version: **
Question:
How to use non-blocking method instead of blocking method in PSoC™ 4 flash?
Answer:
When executing flash erase or write action, the low-level driver uses blocking write method, disables all CPU interrupts until the end of the operation. Sometimes, the system needs to use non-blocking write. The following steps show how to use the non-blocking method using the CY8CKIT-041 Demo Kit:
1. Add the following lines of code to main.c, and make sure to set IMO to 48 Mhz in the *.cydwr clocks.
#define SPC_INT_IRQ 9u //the SPC interrupt No. follow the table
PSOC series |
SPCIF IRQ |
PSOC 4000S |
9 |
PSOC 4100S |
12 |
PSOC 4100S plus |
15 |
#define REG(addr) (*((volatile uint32 *) (addr)))
#define CPUSS_CONFIG_REG REG( 0x40100000 )
extern void SpcIntHandler();
void main()
{
…
CyIntSetVector(SPC_INT_IRQ,SpcIntHandler);
CyIntSetPriority(SPC_INT_IRQ,3);
CyIntEnable(SPC_INT_IRQ);
/* Set CPUSS_CONFIG.VECS_IN_RAM because SPC ISR should be in SRAM */
CPUSS_CONFIG_REG |= 0x00000001;
…
2. Go to Project à Build Settings. In the Build Settings dialog, set Skip Code Generation to False. Then, compile the project to generate the low-level driver.
3. Add the lines of code in red in the current *.ld file:
.data : ALIGN(8)
{
__cy_region_start_data = .;
KEEP(*(.jcr))
*(.got.plt) *(.got)
*(.shdata)
*(.data .data.* .gnu.linkonce.d.*)
. = ALIGN (8);
*(.ram)
KEEP(*(.sramCode))
. = ALIGN (8);
_edata = .;
} >ram AT>rom
4. Define and assign the following three functions to the RAM section of the flash.c file.
/* Variable to keep track of how many times SPC ISR is triggered */
uint32 iStatusInt = 0;
CY_SECTION(".sramCode") __attribute__((used))
void DoStuffRunningInSram(void)
{
CY_NOP;
}
CY_SECTION(".sramCode") __attribute__((used))
void SpcIntHandler(void)
{
volatile uint32 parameters[1];
/* Write key1, key2 parameters to SRAM */
parameters[0u] = (uint32) (((uint32) CY_FLASH_KEY_TWO(0x09) << CY_FLASH_PARAM_KEY_TWO_OFFSET) | CY_FLASH_KEY_ONE);
/* Write the address of key1 to the CPUSS_SYSARG arg */
CY_FLASH_CPUSS_SYSARG_REG = (uint32) ¶meters[0u];
/* Write the API code = 0x09 to the CPUSS_SYSREQ.COMMAND
* register and assert the sysreq bit */
CY_FLASH_CPUSS_SYSREQ_REG = CY_FLASH_CPUSS_REQ_START | 0x09;
/* Number of times the ISR has triggered */
iStatusInt ++;
}
/*******************************************************************************
* Function Name: CySysFlashWriteRow
****************************************************************************//**
*
* Erases a row of Flash and programs it with the new data
********************************************************************************/
CY_SECTION(".sramCode") __attribute__((used))
uint32 CySysFlashWriteRow(uint32 rowNum, const uint8 rowData[])
{…}
5. Set the other interrupt, such as the 2 ms timer interrupt service routine in main.c,. Add the following code. The CPU will run into this handler every 2 ms.
CY_SECTION(".sramCode") __attribute__((used))
CY_ISR(Isr_Timer)
{
/* Clear the TCPWM terminal count interrupt */
Timer_ClearInterrupt(Timer_INTR_MASK_TC);
LED_Blue_Write(~LED_Blue_Read());
msCount++;
if(msCount >= 2)//////1000
{
/* Toggle the green LED state */
LED_Red_Write(~LED_Red_Read());
msCount = 0;
secFlag = 1;
}
Assign the API in the interrupt handler to the RAM: