Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Oscillation Stabilization Wait Time in Traveo S6J3XXX Series MCUs – KBA228170

Oscillation Stabilization Wait Time in Traveo S6J3XXX Series MCUs – KBA228170

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: ShusakuS_56           Version: **

Translation - Japanese: Traveo S6J3XXXシリーズMCUの発振安定待ち時間 – KBA228170 - Community Translated (JA)

Question:

Can I check the completion of the “High-Speed CR/Low-Speed CR/Main/Sub Clock” oscillation stabilization wait time by Source Clock Timer?

Answer:

Yes. The following registers become ‘1’ after the clock oscillation stabilization wait time.

- High-Speed CR Clock: SYSC_FCRCTSTR.INTF
- Low-Speed CR Clock: SYSC_SCRCTSTR.INTF
- Main Clock: SYSC_MOCTSTR.INTF
- Sub Clock: SYSC_SOCTSTR.INTF

For more details, see the Source Clock Timer section in the following documents:

- S6J3110: S6J3110 Series 32-bit Microcontroller Traveo™ Family Hardware Manual
- S6J3120: S6J3120 Series 32-bit Microcontroller Traveo™ Family Hardware Manual
- S6J3200: 32-Bit Microcontroller Traveo™ Family S6J32XX Series Hardware Manual Platform Part
- S6J3300/3350/3360/3370/3400/3510: 32-Bit Microcontroller Traveo Family S6J33xx, S6J34xx, S6J35xx Series Hardware Manual Platform Part

Notes: This KBA applies to the following series of Traveo MCUs:

S6J3110

S6J3120

S6J3200

S6J3300

S6J3350

S6J3360

S6J3370

S6J3400

S6J3510

0 Likes
303 Views