Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

OTA2 Reliability for Battery-operated Wireless Devices - KBA231150

OTA2 Reliability for Battery-operated Wireless Devices - KBA231150

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Version: **

Translation - Japanese: バッテリー駆動のワイヤレスデバイスのOTA2信頼性 - KBA231150 - Community Translated (JA)

To guarantee a reliable OTA2 operation for battery-operated wireless devices such as CYW43907 and CYW54907, it is recommended to check the battery level before executing the OTA2 extract operation.

In /43xxx_Wi-Fi/apps/snip/ota2_extract/ota2_extract.c, the CHECK_BATTERY_LEVEL_BEFORE_OTA2_UPGRADE macro instructs the function to ensure that the battery level is checked before calling the OTA2 extract function. The battery level is checked using the platform_check_battery_level(CHECK_BATTERY_LEVEL_OTA2_UPGRADE_MINIMUM) function. You should customize this function according to your battery circuit design. It contains function calls to measure the battery level.

CHECK_BATTERY_LEVEL_OTA2_UPGRADE_MINIMUM is a user-defined constant which indicates the minimum battery level necessary to perform an OTA2 operation. If the measured battery level is below this value, the platform_check_battery_level() function will return an error; the OTA2 extract operation will not proceed. The CHECK_BATTERY_LEVEL_BEFORE_OTA2_UPGRADE macro can be defined in wiced_defaults.h to enable this feature.

The code snippet of ota2_extract.c is shown below. The macros and functions used for checking the battery-level are highlighted.

void application_start( )

{

    wiced_result_t              result;

    extractor_extract_result_t  extract_result;

    platform_dct_ota2_config_t  dct_ota2_config;

    /*

     * Initially:

     * We don't use the normal wiced_init(), as we don't want wiced_wlan_connectivity_init( ); unless we are running SoftAP

     * We don't use wiced_core_init(), as we don't want to use wiced_platform_init( ), as the filesystem may be invalid, and we don't want to assert

     */

platform_init_external_devices();

    /* initialize DCT mutex */

wiced_dct_init();

OTA2_EXTRACT_PRINTF(("\r\nHi, I'm the OTA2 extraction app (ota2_extract).\r\n"));

    extract_result = EXTRACT_RESULT_OK;

    if ( ota2_extract_check_battery_level() != WICED_SUCCESS)

    {

        extract_result = EXTRACT_RESULT_ERROR_BATTERY_LOW;

    }

The function definition of ota2_extract_check_battery_level() is shown below (also in ota2_extract.c😞

/* Returns WICED_ERROR if battery level considered too low */

wiced_result_t ota2_extract_check_battery_level( void )

{

#ifdef CHECK_BATTERY_LEVEL_BEFORE_OTA2_UPGRADE

    /* check for battery level before doing large amount of writing */

    if (platform_check_battery_level(CHECK_BATTERY_LEVEL_OTA2_UPGRADE_MINIMUM) != WICED_SUCCESS)

    {

        /* check_battery_level() failed */

        return WICED_ERROR

    }

#endif /* CHECK_BATTERY_LEVEL_BEFORE_OTA2_UPGRADE */

    return WICED_SUCCESS;

}

0 Likes
170 Views
Contributors