Negative gate-source bias response of Smart-7 devices
Community Manager
Dec 09, 2021
01:29 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Dec 09, 2021
01:29 AM
Is it possible that PROFET+2 and SPOC+2 devices could lose control of the Gate/input signal when exposed to a negative gate to source bias. e.g. If the device has an open circuit (gate/input is near zero volts (commanded OFF) and the source is pulled high via a current source on the output used for open circuit detection, or if the source/output is shorted to battery).
- Tags:
- PROFET+2_12V
- SPOC+2
Rate this article: