- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Motor System IC - TLE9560/61/62 What is the benefit of configuring separately the cross-current and blank times for the active and for the freewheeling MOSFETs?
During PWM operation of the external half-bridges, the turn-on and the turn-off of the active MOSFETs cause a significant variation of the drain-source voltaSolvege (VDS) from about ~VS to ~ GND and from ~GND to ~VS. Therefore in some applications, the turn-on and turn-off time of the active MOSFET must be long enough for a good electromagnetic emission (EME).
In contrast the turn-on and turn-off of the freewheeling (FW) MOSFETs cause only a small variation of VDS. This variation is equal to the forward voltage of the body diode of the MOSFETs. Therefore the turn-on and turn-off phases of the FW MOSFET can be shorter, without significant penalties in terms of EME.
The different turn-on and turn-off times of the FW and of the active MOSFETs require a separate setting for the cross-current protection time and blank times for the FW and for the active MOSFETs.
Refer to these e-learnings for more information: https://www.infineon.com/cms/media/eLearning/Automotive/adaptive-MOSFET-control/
https://www.infineon.com/cms/media/eLearning/Automotive/advanced-motor-control-intro/