Methods to Upgrade Firmware on CCG3 Devices
Anonymous
Not applicable
Feb 02, 2016
10:36 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Feb 02, 2016
10:36 PM
What are the methods to upgrade firmware on CCG3 devices?
- The firmware on CCG3 devices can be upgraded using one of the following methods:
-
Using SWD lines along with the PSoC Programmer software and MiniProg3 device (click here to purchase) for any application in general.
-
Using I2C bootloader, which is supported for PC/Tablet/mobile phone applications. The application firmware can be upgraded via the I2C bootloader from an applications processor (in the case of tablets and mobile phones) or an embedded controller in the case of PC applications.
-
Using the bootloader supported over CC line for power adapter, power bank, and active cable applications.
All firmware upgrades are supported over the EZ-PD Configuration Utility and a CY4501 CCG1 host board.
Version: *A
Translation - Japanese: CCG3 デバイスのファームウェアを更新する方法 - KBA210974 - Community Translated (JA)
Labels
- Tags:
- ccg
- CCG3 Devices
- cortex-m0
- device programming
- ez-pda ccg3 type-c port controller
- failsafe
- firmware upgrade CCG3
- flash
- non-volatile
- non-volatile memory
- production programmer
- program
- programmable
- programming
- psoc programmer
- PSoC Programmer software
- reprogrammable
- type ez-pd™ ccg3
- usb type-c
- usb-c and power delivery
Rate this article: